U.S. Air Force Base Undergoes Energy Modernization Project, Will Save $1.7 Million Annually

Kunsan Air Base, a U.S. Air Force Base located in South Korea recently announced a $28 million infrastructure modernization project in conjunction with Honeywell that is expected to generate approximately $1.7 million in annual energy savings.

According to Honeywell, the project includes facility upgrades that aim to help improve infrastructure and equipment reliability while lowering the base’s annual energy consumption by more than 18% and water consumption by over 7%.

See full article.