/content/hbtbt/ca/fr/search-results.html

    Valves de régulation indépendante de la pression

    Celeris Valves

    Discontinué

    The Phoenix Controls Celeris family of valves are used whever high speed actuation is required. Typically used in wet chemistry applications where fume hoods are present, Celeris is used to ensure safety of the user at the fume hood.

    Aperçu
    Ce produit n’est plus fabriqué.
    Honeywell fournira un support produit jusqu'à.

    The VALVE-CELERIS is a control valve by Phoenix that is used whever high speed actuation is required. Typically used in wet chemistry applications where fume hoods are present, Celeris is used to ensure safety of the user at the fume hood.

    Celeris is a highly configurable control platform that builds on the accuracy of the Phoenix Controls venturi valve. The valves provide uncompromised fume hood containment and directional airflow ensuring complete safety to the user. Phoenix Controls valves do not require straight duct runs, either upstream or downstream. This reduces the overall cost to the user. The valves have high turndowns that provides opportunities to save energy. All these features make the valve cost efficient, reliable and the performance, efficient.

    Features & Benefits:
    • Operator safety
    • Room pressurization
    • Ventilation
    • Comfort
    • Reliability
    Caractéristiques

    Autres

    • Brand
      • Phoenix Controls

    Autres

    • Brand
      • Phoenix Controls
    • Brand : Phoenix Controls