HONEYWELL DEPLOYS BUILDING MANAGEMENT SYSTEM AND ENHANCES SECURITY SYSTEM AT NEW ALTERNATIVE CARE FACILITY AT MIAMI BEACH CONVENTION CENTER

  • ·Upgraded existing building management system to add HEPA filtration
  • Installed fire and life safety system as well as upgrades to security access control system

 

Miami, May 4, 2020 – Honeywell (NYSE: HON) today announced it worked with Miami Dade County and City of Miami Beach leaders to help deploy the new Alternative Care Facility at the Miami Beach Convention Center (MBCC) as part of the county’s COVID-19 response and preparedness plan. Honeywell Building Solutions worked with the MBCC, the city and county, the U.S. Army Corps of Engineers, B&I Mechanical, construction firm Robins and Morton and others on the project.

The project converted 250,000 square feet of the MBCC into a 450-bed alternative care facility that features 50 ICU isolation rooms. The project construction and installation were completed in just two and a half weeks following a 24/7 focus on the build.

“The effort to transform the MBCC into an alternative care facility in just over two weeks’ time has truly been an awesome feat of teamwork, trust and partnership among all parties involved,” said Freddie Peterson, General Manager, Miami Beach Convention Center. “We’ve transformed a space typically used to feature some of the world’s largest events and conventions into a fully operational field hospital to support the COVID-19 pandemic.”

Honeywell focused on upgrades to the site’s building management system (BMS) to make sequence changes for desired air exchange to improve the building's circulation of fresh air and the monitoring of the HEPA filter banks. Constant outside airflow exchange was improved by the ramp up of the chiller plants and sequence of operations changes as well as modifications to exhaust fans and relief dampers to ensure negative pressurization in the occupied areas. Honeywell also made updates to the MBCC security system focused on access control to regulate access to restricted areas and updated the CCTV system.

“Our team is proud to work with the MBCC, the U.S. Army Corps of Engineers and all parties involved to quickly and safely commission the site,” said Jose Simon, vice president and general manager of projects, Honeywell Building Solutions. “Our focus has been on the building management system, airflow and chiller management – you have dramatically different airflow needs when you look at a large open space like the MBCC than you would with a traditional hospital setting. We adjusted the BMS for more fresh air exchanges and added overlays to improve the overall airflow.”  

Patient care is managed by Florida Emergency Management, Florida National Guard medical teams and private contractors at the site if the local hospitals become overwhelmed.

About Honeywell Building Technologies

Honeywell Building Technologies (HBT) is a global business with more than 23,000 employees. HBT creates products, software and technologies found in more than 10 million buildings worldwide. Commercial building owners and occupants use our technologies to ensure their facilities are safe, energy efficient, sustainable and productive. For more news and information on Honeywell Building Technologies, visit http://www.honeywell.com/newsroom.

About Honeywell

Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

About MBCC

The Miami Beach Convention Center (MBCC) is the centerpiece to Miami Beach’s meetings and conventions industry. Re-imagined following a $620-million-dollar renovation, the expanded MBCC includes a new 60,000 square-foot Grand Ballroom, almost 500,000 sq. ft. of exhibition space, an expanded Grand Lobby, pre-function areas that are bathed in natural light, up to 84 breakout rooms, almost 2,100 miles of cabling to support all IT communications, $7.1 million dollars’ worth of art curated by the City of Miami Beach Art in Public Places program, a new six-acre public green space that can serve as incremental event space, and much, much more. For general information, visit www.miamibeachconvention.com or call 786-276-­2600.

Megan McGovern

Honeywell Building Technologies

+1 (404) 216-6186

Email

Sabrina Anico

MBCC

+1 786-390-3568

Email