https://buildings.honeywell.com/us/en/search-results.html

Antennas & Receivers

WLan Smile Connect Stick

The WLan Smile Connect stick can be used instead of the network cable connection from the router to the bridge. The Wlan is connected via USB interface.

The WLan Smile Connect stick can be used instead of the network cable connection from the router to the bridge. The Wlan is connected via USB interface. In the case of longer distances, standard WiFi repeaters can be used to increase the reception capacity of the stick WLan.

Others

  • Brand
    • Honeywell

Others

  • Brand
    • Honeywell
  • Brand : Honeywell
Image
SKU
Description
alt
SCW-10
WLan Smile Connect Stick, 802.11b/g/n, 20g