Dimmers
Hometronic Dimmer module
The HD30 is a dimmer module by Honeywell which is designed for adjusting the brightness of the connected electric light bulbs of high and low-voltage HV halogen lamps with an inductive iron-core transformer.
The HD30 is a dimmer module by Honeywell which is designed for adjusting the brightness of the connected electric light bulbs of high and low-voltage HV halogen lamps with an inductive iron-core transformer.
The dimmer module is used in conjunction with the HCM 200 Hometronic Manager in a Hometronic system. The HD30 is intended to be surface-mounted on a flush mounted distribution box. There is no need to change the existing electrical wiring system. The dimmer module can adjust the brightness of the connected electric lights not only with the existing light switches but also independently of the wiring via the HCM 200 Hometronic Manager. When configured with the HCM 200 then user can also control the brightness of the lights by means of a timing program. The HD30 will switch the connected lights on or off, or dim them, while the user are away from the house. The dimmer module not only saves the energy but also extends the life of the electric bulbs.
Features & Benefits:- No need to change the existing electrical wiring system
- Can be upgraded according to individual user requirements
- Automate turn on/off or dimming of the electric bulbs