Specialty Modules
Vigilon Network Card
The fibre network card allows fast message passing to the network. The card must be plugged into the backplane of the panel or node in a dedicated slot.
The fibre network card allows fast message passing to the network. The card must be plugged into the backplane of the panel or node in a dedicated slot. The fibre optic cables connect directly to sockets on the card. There are two builds of the fibre network cards for secure EN54 and BS Vigilon network.
Using the Fibre Optic Network card VIG-NC-DOM-FO up to 64 smaller networks can be connected to form a secure domain. The Fibre Optic cable distance between nodes of the smaller networks can be up to 2Km. The entire system can have up to 200 panels/nodes.
Features & Benefits:- 200 panels/nodes
- 64 smaller networks can be connected to form a secure domain
- Fibre network cards for secure EN54 and BS Vigilon networks
- EN54
Others
- Brand
- Gent
Others
- Brand
- Gent
- Brand : Gent
Image
SKU
Description
VIG-DOM-FIBRE
Network Card: 2211-141: Factory Fitted: Domain Bridge