You are browsing the product catalog for
You are viewing the overview and resources for
- ESSER by Honeywell
- Industrial
Industrial
Technological fire protection for production halls in stainless steel pipe...
The family-owned company fischer Edelstahlrohre (stainless steel tube production), based in Achern, Germany, relies on professional fire protection in its production halls so as not to endanger production and know-how worthy of protection. The Offenburg-based FREWA Sicherheitstechnik GmbH was commissioned to install suitable fire protection components. By using a wide range of products of the traditional brand ESSER, almost every fire risk is covered.
Huge areas, high-quality machinery, few personnel
Unlike most other object types, the protection of material assets is top priority in the industry. The avoidance of false alarms is of great importance because a loss of production or even an operational failure could have far-reaching consequences. A special challenge for the fire alarm system is that diverse disturbance variables are nothing unusual in industrial buildings.
Risk management for the chemical and pharmaceutical industry
The chemical and pharmaceutical industry has very specific security needs that differ significantly from those of other industries. Explosion-protected areas, special requirements for the operational safety of the plants, 100% availability - all this must be covered by integrated hazard management.
Intelligent early fire detection in wind turbines
Due to the highly fluctuating and aggressive environmental conditions, wind turbines are a place of operation that places high demands on fire detectors.
Copyright © 2026 Honeywell International Inc.