Silent Knight Software/Firmware Updates
Stay up-to-date with the latest Silent Knight programming software and product firmware to ensure you have all the latest product features and performance improvements.
Latest Honeywell Fire Software Suite with 6000 Series firmware bundle
Honeywell has bundled the latest Honeywell Fire Software Suite (HFSS 8.1.0.11) with 6000 Series Firmware Version 7.0.0.21 due to the integration of password usability improvements.
Honeywell Fire Software Suite (HFSS)
HFSS is the latest Honeywell Silent Knight programming software designed for the 6000 Series line of fire alarm control panels. HFSS expands on the previous SKSS platform and is required for programming the 6700, 6808, 6820 and 6820EVS panels. HFSS has been updated to include newly released products and makes it easier than ever before to program new features. Note: HFSS is designed for use with the 6000 Series panels, but now has an importer tool to convert legacy SKSS files to HFSS files. Apart from converting legacy to current panels, SKSS should continue to be used for the previous 5000 Series line of fire alarm control panels.
Changes in version 8.1.0.11
- Supports new firmware 7.0.0.21
- Supports upcoming panel Variants 6808U, 6820U, IFP-300U and IFP-1100U
- Single Sign on Support with other CLSS connected tools
- Refresh token to extend the offline token expiry to 90 days
- Tool supports conversion of panels:
- 6808 -> 6808U
- 6820 -> 6820U
- IFP-300 -> IFP-300U, IFP2100, IFP1100U
- IFP-2100 -> IFP1100U
- FCP-300 -> FCP-300U
- New product keyshave been introduced from v8.1 onwards
- Repair for report generation
Previous versions of HFSS
Version 8.0.21.10 - Download
- All 20 user profiles passwords can be fetched from the tool by providing the current “Admin 1” Password.
- Along with user profile passwords, current Computer Access Number is required to fetch all passwords.
- User can modify any of the User Profile passwords along with Computer Access Number and submit back to the panel.
- Fire Fighter key passcode can’t be changed.
- Upon newly setting the password for any profile, panel will enable the user profile if it is disabled. Similarly, removing the password would disable the user profile in the panel.
- Added a link to Honeywell’s Privacy Statement while logging into the tool
- Minor Bug fixes
Version 8.0.11.0 - Download
- NVCM module is now available for 6820EVS panel type while adding SBUS modules
- NVCM module is now being supported for 6820EVS panel
- SKSS Importer changes can convert VCM to NVCM while importing 5820EVS files to 6820EVS
Version 8.0.0.0
- User can change the existing internal annunciator between smaller and new larger display for 6808 and 6820 type panels.
- SKSS Importer changes to set large display to 6808 and 6820 panel types.
Version 7.0.350.0
- Now supports new displays on 6808 & 6820
6000 Series Firmware
The Honeywell Silent Knight 6000 Series addressable fire alarm control panels were designed to accept panel firmware updates. Updating the panel to the latest released firmware is highly recommended in order to fix known issues and add additional features and product support.
6000 Series Firmware Version 7.00.21 (Note: HFSS upgrade to 8.1.0.11 required)
Previous versions of 6000 series firmware