/content/hbtbt/ca/fr/search-results.html

    Phoenix Controls And SLD Technology Launch First-Of-Its-Kind Solution To Manage Critical Healthcare Environments

    Phoenix venturi valves and data visualization software suite helps create a stable zone of asepsis in operating suites and is now available in SLD modular AirFRAME® ceiling unit, supports D4Z® design methodology

    ACTON, Mass., – October 17, 2022 – Phoenix Controls, a leader in precision airflow control solutions for critical environments, announced today it is working with SLD Technology, a manufacturer of fully integrated modular ceiling systems for healthcare facilities, to help create a stable zone of asepsis in operating suites through enhanced environmental controlled airflow. The enhanced environmental controlled solution can help manage hospital-acquired infections (HAI) and further supports the healthcare industry’s adoption of D4Z[i] (Design for Zero infections), a strategy to minimize hospital infections, improving the healing environment while creating energy efficiencies for hospitals​.

    Five to 10% of patients[ii] contract at least one HAI during their stay in a hospital. Not only is this a problem for patients recovering from surgery or illness but it also costs the U.S. healthcare system an estimated $3.5 to $10 billion annually[iii]. To prevent these outcomes, critical environments like operating rooms, intensive care units and laboratories must maintain sterilization, and as such, healthcare facilities are incorporating measures like environmental monitoring and performance-based airflow control strategies to help limit the spread of airborne pathogens and improve indoor air quality (IAQ) during dynamic conditions.

    SLD (Single Large Diffuser)’s flagship offering AirFRAME®, a modular ceiling system for healthcare, now features Phoenix Controls’ venturi valves, peripherals and data visualization software suite Vision CE which incorporates the BEACON active infection prevention algorithm. The integrated solution enables real-time IAQ data visualization to help healthcare providers, like surgeons and infection preventionists, improve decision-making and patient outcomes. Installation and maintenance of the solution will be led by Phoenix Controls’ dealers and channel partner network.

    “This integration is designed to help improve the quality of critical healthcare environments, while also supporting operational savings to a hospital’s bottom line,” said Dave Rausch, director of strategic partnerships, Phoenix Controls. “Managing infections may mean fewer unexpected costs per surgery. Additionally, as the solution is mechanically pressure independent, it requires less maintenance than a traditional HVAC valve and operates more efficiently.”

    “Our integrated solution with Phoenix Controls removes the guesswork of sourcing best-of-breed technologies for healthcare facilities looking to optimize their critical environments,” said Kevin Schreiber, founder and president of SLD Technology. “Our combined expertise and application knowledge can help drive improved outcomes for both patients and hospitals.”

    Since 1985, Phoenix Controls’ precision airflow control systems have been used in critical environments, such as pharmaceutical companies, universities, hospitals and government research facilities. With a global network of partners to assist with design and space requirements, Phoenix Controls provides a complete system solution.

    SLD Technology’s AirFRAME modular ceiling systems feature unidirectional, low-turbulence airflow for close temperature and humidity control and airborne contaminant removal. The AirFRAME system is the first, and only, modular ceiling system to incorporate IndigoClean visible light disinfecting technology. The plug-n-play system integrates ambient lighting, med-gas, HVAC, monitoring and structural equipment mounting elements in complete, factory-built modules that both compress construction schedules and enhance patient outcomes.

    About Phoenix Controls
    ​Phoenix Controls is a leading provider of precision airflow control solutions for critical environments, delivered with advanced technology to customers throughout the world.

    About SLD Technology
    SLD Technology, Inc., designs and manufactures systems and components that simplify design, speed installation, and deliver superior performance in hospitals and other healthcare facilities. Its applications support operating rooms, imaging rooms procedure rooms, exam rooms, and pharmacies with complete, factory-built modules.

    Learn more about how Honeywell’s integrated technologies support healthcare operations in an interactive experience.

     

    [i] Designed 4 Zero, Is your hospital Designed 4 Zero?, 2022. [Accessed August 3, 2022]

    [ii] National Conference of State Legislatures, Frequently Asked Questions. [Accessed July 29, 2022]

    [iii] American College of Surgeons and Surgical Infection Society, Surgical Site Infection Guidelines, 2016 Update. January 2017. [Accessed July 29, 2022]