/content/hbtbt/gb/en/search-results.html
    Scheduled Maintenance: This site will be temporarily down for scheduled maintenance on February 21, 2026 6:30 AM - 7:00 AM UTC (1:30 AM - 2:00 AM EST | 12:00 PM - 12:30 PM IST | 7:30 AM - 8:00 AM CET | 6:30 AM - 7:00 AM GMT). We appreciate your patience during this time.

    Papieri Cham

    Heading towards a renewable future

    From paper mill to living space

    The Cham paper mill site in Switzerland is being transformed into a new residential and working neighborhood.

    The site aims to be energy-efficient, climate-neutral, and sustainable. In fact, approximately 40% of the electricity needed will be generated on-site through photovoltaic systems and a river power plant. A key feature will be the energy network from Saia Burgess Controls (SBC) and MST Systemtechnik, which will connect the energy sources on the site using innovative solutions.

    THE CHALLENGE

    The core of the implementation is the site-wide energy network by Saia Burgess Controls (SBC) together with MST Systemtechnik which connects available energy sources directly on site through innovative solutions. Renovating the historic buildings on this site presents unique challenges, particularly due to unforeseen obstacles with listed buildings. This is where the flexibility of Saia PCD control systems becomes invaluable. Our systems allow for seamless integration of third-party systems, significantly easing the renovation process.

    THE SOLUTION

    At the field and control level, over 80 Saia PCD controllers and 70 control cabinets will be integrated by the expected completion date in 2035, and the system topology is correspondingly complex. The Saia PCD3 controller used is particularly robust and designed for demanding applications. Up to five integrated communication interfaces are available and the plug-in modules allow individual expansion, a detail that is worth its weight in gold for projects that require a high degree of flexibility. In addition, investing in a flexible, high-quality system with a long-life cycle, for which Saia PCD controllers are known, also makes sense financially.

    RESULTS

    Over 80 Saia PCD controllers have been integrated at both the field and control levels, contributing to a complex system topology. In fact, depending on the situation, geothermal energy or river water is used for efficient heating and cooling. The collaboration between MST-Systemtechnik and SBC has been successful.

    HIGHLIGHTS
    • Sustainability and climate neutrality as core focus
    • Challenge: Coordinating energy sources (hydropower, solar, geothermal, heat pumps)
    • Saia PCD3 controller ensures reliable performance
    • Financial benefits through high-quality and long-life cycle systems