/content/hbtbt/ae/en/search-results.html

    gateways

    Notifier Wireless FDAS - Gateway

    Wireless Gateway

    Overview

    The Notifier Wireless Fire Detection System can be applied in many situations that are problematic for traditional wired detectors. In cases where areas of a building are difficult or impossible to wire, visually sensitive, or have restricted access. Each Wireless detector develop “parent-child” communication links with other detector in the mesh, so that a message originating from a remote detector “hop” to the closest parent detector, and then to successive parent detector until the message reaches gateway. Alternate paths are also identified and supervised by the wireless protocol providing approved Class A wireless communication. If a detector does not have an established communication path with adequate signal strength, an additional detector such as a may be installed in between so that it will act as a repeater.

    The Notifier Wireless gateway system supports up to 31 detectors: 1 Wireless gateway. The maximum number of gateways on a system is limited upto 3, irrespective of no of SLC on the FACP

    Features & Benefits:
    • Wireless mesh protocol specifically for fire and life safety systems
    • Operates in 865-867 MHz frequency.
    • Patented cascading-wave mesh operation provides a verification of redundant communication paths that has been approved for Class A.
    • In the event that a communication path is interrupted at any point by a change in the radio environment, the wireless mesh system will use the redundant or backup communication path.
    • In the event that any links cannot be established with sufficient signal strength, any Wireless detector can be added to act as a repeater, eliminating the need for wired repeaters.
    • Each Wireless gateway system support up to 31 detectors: 1
    • wireless gateway.
    • Multiple wireless mesh networks can be installed on the same fire alarm control panel, or on multiple panels in the same area.
    Certifications:
    • UL
    Specifications

    Others

    • Brand
      • NOTIFIER

    Others

    • Brand
      • NOTIFIER
    • Brand : NOTIFIER